Skip to content

Annotating images

ℹ️ Note: The annotation process for instance segmentation is the same as for object detection.

Press the Annotate button in the Pending annotation section. This will take you to the Annotation view in dTag.

Pending annotation

I want to filter which images are included in the Annotation Job You can set up filters and other options by creating an Annotation Job in dTag. On the right, click on the three dots symbol and click Manage domain. Then click on Annotate on the left. Then follow the instructions on how to create an Annotation Job in the dTag tutorial section. Navigating to Annotation Job creation in dTag from dStudio

Annotation overview

To solve the application we want the network to learn the position of glass vials in an image. In order for the network to learn where the objects are, we need to give it examples images containing different kinds of glass vials and show where in the image the different objects are located. This means we have to annotate images, meaning we have to draw a polygon or bounding box around the objects. We can do this in two different ways:

  1. Automatic annotation using the Assisted Object Annotation Tool.
  2. Manual annotation - clicking in the picture.

Option 1 is recommended since it is typically faster than a manual annotation. For the cases where the Assisted Object Annotation tool struggles, you might need to use the manual approach. You can switch between the two approaches on the fly.

Approach 1: Automatic annotation using the Assisted Object Annotation tool

Rather than having to manually click all the points of a polygon to make an annotation, it is recommended to use Assisted Annotation. Choose one of 3 assisted annotation modes to create a mask and save it as polygons. When the blue mask appears, choose a segmentation class and save the polygon(s).

There are hotkeys for all the Assisted Annotation Modes

Keymaps
  • Shift+a: Activate Assisted Object Annotation Tool.
  • Left mouse button: Positive prompt.
  • Right mouse button: Negative prompt.
  • Ctrl+Left mouse button on a prompt point: delete prompt.
  • Esc key: delete all prompts/clear mask.
  • Spacebar: Accept Mask and generate a polygon.
  • h: show/hide all objects

Point Prompts

  • You can choose the point mode for images with only a few of the same objects.

Enable the Assisted Object Annotation Tool

  • Select the object class you want to annotate.

  • Click on the object in the image to create a prompt (blue dot). A mask (blue overlay) will be suggested. Add more prompts if the object is not masked fully.

  • In case the proposed mask covers more than the object, click with the right mouse button to add a negative prompt (red dot) on that area to indicates that this part of the mask is not part of the object.

  • Press the Spacebar to accept the mask. This will transform the mask into a polygon. You can edit this polygon if you wish to make any adjustment, but you need to switch back to Manual Editing (shift+a) to add or move polygon points.

Annotating with the Assisted Object Annotation Tool

  • Click the eye icon next to the class to hide all objects of this class.
Keymaps Point Prompts
  • Left mouse button: Positive prompt.
  • Right mouse button: Negative prompt.
  • Ctrl+Left mouse button on a prompt point: delete prompt.

Use this approach to annotate the vials in the image. Once you have annotated all of the vials, press the blue Save button.

First image done

Bounding Box prompts

For images with a lot of the same objects you can use the Bounding Box Prompt

Annotating with the Assisted Annotation Bounding Box

or the Text Prompt. Annotating with the Assisted Annotation Text

Proceed to the More on how to make annotations section.

Approach 2: Manual annotation - clicking in the picture

To start, click the appropriate class in the left panel and start clicking on the image to create the shape. Click on the first point to close the shape.

Manual annotation

Continue this proceedure for the other glass vials in the image. Remember to pick the right class on the left hand side before making the annotation. If you need to change class of an annotation, you can do so by pressing the three dots next to the annotation and choose another class.

Change class

One object can also consist of multiple shapes, in case a part of the object is partly obstructed or hidden. Add a second shape to one object by selecting the object and alt+click anywhere on the image to append the shape to the existing object.

Append to existing object - Manual annotation

After you have labelled all vials in the image, save the image by pressing the blue Save button.

Proceed to the More on how to make annotations section.

More on how to make annotations

Instances

If an image contains multiple objects, it is said to have multiple instances. For example, if there are two green vials we can also say that there are two instances of green vials in the image. The number of instances per class is displayed next to the class name on the left.

Number of instances per class

Changing multiple objects at once

You can merge, delete or change the class of multiple objects at once. Deleting: If you are not happy with the created polygons you can select them either in the list or in the image (not in Points mode!) and click on the delete button at the top of the objects list.

Delete instances per class

Merging: If an object is split up into multiple polygons by mistake you can select them in the objects list and click on the merge button.

Merge instances per class

If an object consists of too many polygons you can delete it and redo the annotation.

Switching the class:

Class Switching

Order of annotation shapes

It is very important to maintain the order of the segmentations in the image. The order in the object list is the order of the segmentation paths in the image. The shape in the background needs to be the shape on the bottom of the object list.

To change the order, select an object in the objects list and drag it to the correct position in the list. Change order of annotations

You can get details for how to navigate the image, edit segmentations, use the Assisted Object Annotated tool and different shortcuts by pressing the question mark icon on the top right.

Help icon

Settings

Most likely you will not need to tweak any of the two sliders, but if you encounter one of the following situations here is what you need to do:

Issue 1: Only a few objects are found and you need to iterate to get all objects, but you don't want duplicate annotations OR you have already annotated some objects but you don't want duplicates.

Issue 2: You see "Results filtered" when trying to create another annotation of an already annotated object.

Solution: Adapt the Existing Object Overlap Threshold to prevent masks that include already annotated objects. It will reject any mask that overlaps with an already annotated object by more then x% of area.

Existing Object Overlap Threshold

Issue: The masks by the Assisted Annotation Tool find the same object twice or parts of the object plus the actual object.

Solution: You can use the Score-Based Overlap Threshold to make sure only high scoring masks are returned by the Assisted Annotation Tool. It will reject any mask that overlaps with any other returned mask by more then x% of area and has a lower confidence score than the mask in comparison.

It is set to 5% by default so this issue should never occur.

Score-Based Overlap Threshold

Annotate the rest of the images

Annotate the rest of the images in the dataset. Once the annotations are finished, press the "Open in dStudio" button and select the Object Finding tab.

Return to dStudio

Reviewing annotations

Learn more about how to set up an Annotation Job for reviewing annotations in the Review Jobs section.